PROFIdrive Signals

The following PROFIdrive signals are permitted.


  • The PROFIdrive signals are not mapped 1:1 to the AKD2G signals. The unit conversion for PROFIdrive must be used. For more information, see Units.

The predefined standard telegrams are used for accessing the signals or a free mapping is used with telegram 0.

Signal
Number
Signal
Format
PROFIdrive
Signal Name
AKD2G Signal Description
1 WORD STW1 AXIS#.PROFINET.STW1 Controlword 1 can only be mapped at index 0 of AXIS#.PROFINET.​SETPOINTMAP (P915)
2 WORD ZSW1 AXIS#.PROFINET.ZSW1 Statusword 1 can only be mapped at index 0 of AXIS#.PROFINET.​ACTUALVALUEMAP (P916)
3 WORD STW2 AXIS#.PROFINET.STW2 Controlword 2
4 WORD ZSW2 AXIS#.PROFINET.ZSW2 Statusword 2
5 WORD NSOLL_A AXIS#.VL.CMD 16-bit target velocity
6 WORD NIST_A AXIS#.VL.FB 16-bit actual velocity
7 DWORD NSOLL_B AXIS#.FBUS.VL.CMD 32-bit target velocity
8 DWORD NIST_B AXIS#.VL.FB 32-bit actual velocity
9 WORD G1_STW AXIS#.PROFINET.G1STW Sensor 1 Controlword
10 WORD G1_ZSW AXIS#.PROFINET.G1ZSW Sensor 1 Statusword
11 DWORD G1_XIST1 FB#.P 32-bit position value with 12 bits multi-turn
12 DWORD G1_XIST2 FB#.P 32-bit position value with 12 bits multi-turn or error code
21 WORD E_DIGITAL DIN.STATES  
22 WORD A_DIGITAL AXIS#.PROFINET.ADIGITAL Digital output fieldbus states
23 WORD E_ANALOG AIN1.VALUE (AIN#.VALUE) Scaling: mV
24 WORD A_ANALOG AOUT1.VALUE (AOUT#.VALUE ) Analog output 1 fieldbus value, scaling: mV
25 WORD XERR AXIS#.PROFINET.XERR System deviation/position error
26 WORD KPC AXIS#.PROFINET.KPC Position controller gain
28 DWORD XISTA AXIS#.PL.FB 32-bit position value scaled according to position units
32 WORD SATZANW AXIS#.PROFINET.SATZANW Position mode Controlword (MT select/MDI mode)
33 WORD AKTSATZ AXIS#.PROFINET.AKTSATZ Position mode Statusword
34 DWORD MDI_TARPOS AXIS#.PROFINET.MDITARPOS 32-bit target position
35 DWORD MDI_VELOCITY AXIS#.PROFINET.MDIVELOCITY 32-bit target velocity
36 WORD MDI_ACC AXIS#.PROFINET.MDIACC Acceleration
37 WORD MDI_DEC AXIS#.PROFINET.MDIDEC Deceleration
38 WORD MDI_MOD AXIS#.PROFINET.MDIMOD MDI mode. Bit 0:
0: Relative Positioning
1: Absolute Positioning
5025 DWORD   AXIS#.MOTIONSTAT  
5100 WORD   AXIS#.FBUS.ACC Similar to MDIACC but updates keyword directly regardless of controlword.
5101 WORD   AXIS#.FBUS.DEC Similar to MDIACC but updates keyword directly regardless of controlword.
5104 WORD   AXIS#.FBUS.IL.CMD  
5803 WORD   AXIS#.IL.FB  
5829 WORD   AXIS#.IL.LIMITP / AXIS#.IL.LIMITN  
5901 DWORD   AXIS#.PL.ERR  
6104 DWORD   AXIS#.HOME.DIST  
6107 WORD   AXIS#.HOME.MODE  
6311 WORD   AXIS#.MT.FEEDRATE Scaling: 100% per 65535 counts
10008 DWORD   AXIS#.SAFE.​FUNCTIONSTATUS  
23101 WORD   AIN2.VALUE (AIN#.VALUE) Scaling: mV
24151 WORD   AOUT2.VALUE (AOUT#.VALUE ) Analog output 2 fieldbus value, scaling: mV